BFS-PGE-63S4 Release Notes

Product Information

Product: BFS-PGE-63S4

Firmware Version: 2303.0000.039.000

Bugs Fixed

Bug Description
FIRM-7322 Persistent IP is not retained when ethernet cable unplugged and plugged, while camera is powered by GPIO.

Changes

Change Description
FIRM-3979 Added Exposure Time Offset
FIRM-7569 Added Lossless Compression feature

Known Issues

Issue Description
FIRM-2277 BFS-PGE-63S4 reports TransferQueueOverflowCount of 1 when streaming in 100Mb link
FIRM-7862 Maximum Frame Rate feature for Lossless Compression(LLC) is not supported. Firmware only supports fixed frame rate mode in LLC.
FIRM-9205 Reported/actual Exposure Time is 382us more than the set value
FIRM-9025 Occasional corrupt first frame when Adaptive compession is enabled during Lossless Compression