BFS-PGE-70S7 Release Notes

Product Information

Product: BFS-PGE-70S7

Firmware Version: 2309.0000.357.000

Bugs Fixed

Bug Description
F-6057 GVSP reported wrong offset_y in Extended Chunk Data Leader
F-6036 The camera turned into the state which could not send out image data
F-6587 BFS GigE cameras getting stuck in updator mode after port interruptions
F-7404 Chunk serial data is misaligned
F-5310 Bayer pattern changes are not picked up if ISP is off

Changes

Change Description
F-9314 Added Lens Shading Correction (LSC) feature

Known Issues

Issue Description
NA