BFS-U3-13Y3 Release Notes

Product Information

Product: BFS-U3-13Y3

Firmware Version: 1808.0.120.0

Bugs Fixed

Bug Description
41772 Mono8 uses 2x2 binning by default due to ISP Enable being off.
48113 Camera does not busy ACK commands sent when processing current command.
49890 USB3CV Chapter 9 test fails since camera should be classified as camera should be classified as 3.1 not 3.0.
52186 The Mainboard temperature reading is not updating correctly.
53497 Failed to start acquisition after running for an hour.
53848 Prevent color sensors from using adjacent sensor binning.
54380 Requested frame rate is actually 1 line more resulting in a slower frame rate.
F-108 Allocate as many images in frame buffer as allowed.
F-300 Reduce the USB2 bandwidth to the reasonable value(43MB).
F-1582 Fixed setting exposure time in chunk data.

Changes

Change Description
36378 Add SequencerConfigurationReset feature.
49776 Implemented serial port feature.
51007 Added a DeviceTemperatureSelector node, implemented reading the Mainboard temperature.
52286 Capture GPIO state in chunk data.
54078 Rebranded camera vendor name from "Point Grey Research" to "FLIR".
F-1260 Support moving test pattern.
F-1448 Added support for 10-bit pixel formats.
F-1472 Add the usb2 reset function controlled by firmware.

Known Issues

Issue Description
41813 ExposureAuto should be off when ExposureMode is set to TriggerWidth.
48369 Device failed to come back after reboot intermittently on USB2.