You are here: Technical Reference > Event Control > Event Exposure End Data
FLIR

Blackfly®S

BFS-U3-200S6

 

Event Exposure End Data

Category that contains all the data features related to the Exposure End Event.

Summary Table

Name Interface Access Visibility Description
Event Exposure End IInteger RO Expert Returns the unique identifier of the Exposure End type of Event.
Event Exposure End Timestamp IInteger RO Expert Returns the Timestamp of the Exposure End Event.
Event Exposure End Frame ID IInteger RO Expert Returns the unique identifier of the frame (or image) that generated the Exposure End Event.

Event Exposure End Data Features


Event Exposure End

Returns the unique identifier of the Exposure End type of Event.

Property Value
Name EventExposureEnd
Interface IInteger
Access RO
Unit
Visibility Expert
Value 0x9C43

Event Exposure End Timestamp

Returns the Timestamp of the Exposure End Event.

Property Value
Name EventExposureEndTimestamp
Interface IInteger
Access RO
Unit
Visibility Expert

Event Exposure End Frame ID

Returns the unique identifier of the frame (or image) that generated the Exposure End Event.

Property Value
Name EventExposureEndFrameID
Interface IInteger
Access RO
Unit
Visibility Expert

 

8/31/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-200S6
Camera Reference