NConversion | |
▼NCpuUtil | |
CCpuUsageInfo | |
NPerformanceCounter | |
NSecondsCounter | |
▼NSpinnaker | |
►NGenApi | |
►NGenICam | |
►NGUI | |
►NGUI_WPF | |
►NVideo | |
CActionCommandResult | Action Command Result |
CBasePtr | The base class of the SystemPtr, CameraPtr, InterfacePtr, ImagePtr and LoggingEventDataPtr objects |
CBMPOption | Options for saving Bitmap image |
CCamera | The camera object class |
CCameraBase | The base class for the camera object |
CCameraList | Used to hold a list of camera objects |
CCameraPtr | A reference tracked pointer to a camera object |
CCCMSettings | |
CChunkData | The chunk data which contains additional information about an image |
CDeviceArrivalEventHandler | An event handler for capturing the device arrival event |
CDeviceEventExposureEndData | Data Fields for Device Event payload for EventExposureEnd |
CDeviceEventHandler | A handler to device events |
CDeviceEventInferenceData | Data fields for Device Event payload for EventInference |
CDeviceEventUtility | Static helper functions for the device event object class |
CDeviceRemovalEventHandler | An event handler for capturing the device removal event |
CEventHandler | The base class for all event handler types |
CException | The Exception object represents an error that is returned from the library |
CICameraBase | The interface file for base class for the camera object |
CICameraList | Used to hold a list of camera objects |
CIChunkData | The Interface file for ChunkData |
CIDataStream | |
CIDeviceArrivalEventHandler | |
CIDeviceEventHandler | |
CIDeviceRemovalEventHandler | |
CIImage | The interface file for Image |
CIImageEventHandler | |
CIImageList | The interface file for ImageList class |
CIImageListEventHandler | |
CIImageProcessor | The interface file for ImageProcessor class |
CIImageStatistics | The interface file for image statistics |
CIInterface | The interface file for Interface |
CIInterfaceArrivalEventHandler | |
CIInterfaceEventHandler | |
CIInterfaceList | The interface file for InterfaceList class |
CIInterfaceRemovalEventHandler | |
CILoggingEventHandler | |
CImage | The image object class |
CImageEventHandler | A handler for capturing image arrival events |
CImageList | Used to hold a list of image objects |
CImageListEventHandler | A handler for capturing image list arrival events |
CImageProcessor | Image post processing class for converting a source image to another pixel format |
CImagePtr | A reference tracked pointer to an image object |
CImageStatistics | Represents image statistics for an image |
CImageUtility | Static helper functions for the image object class |
CImageUtilityCCM | Static function to create color corrected images from an image object |
CImageUtilityHeatmap | Static functions to create heatmap images from image objects of pixel format Mono8 and Mono16 |
CImageUtilityPolarization | Static functions to create polarization images from image objects of pixel format Polarized8 and BayerRGPolarized8 |
CInferenceBoundingBoxResult | An inference bounding boxes object which holds information about the detected bounding boxes |
CInferenceBoxCircle | |
CInferenceBoxRect | Inference Bounding Box Type Data Structures |
CInferenceBoxRotatedRect | |
CInterface | An interface object which holds a list of cameras |
CInterfaceArrivalEventHandler | An event handler for capturing the interface arrival event |
CInterfaceEventHandler | A handler to device arrival and removal events on all interfaces |
CInterfaceList | A list of the available interfaces on the system |
CInterfacePtr | A reference tracked pointer to the interface object |
CInterfaceRemovalEventHandler | An event handler for capturing the interface removal event |
CISpinnakerGPU | The interface file for SpinnakerGPU class |
CISystem | The interface file for System |
CISystemEventHandler | |
CJPEGOption | Options for saving JPEG image |
CJPG2Option | Options for saving JPEG2000 image |
CLibraryVersion | Provides easier access to the current version of Spinnaker |
CLoggingEventData | The LoggingEventData object |
CLoggingEventDataPtr | A reference tracked pointer to the LoggingEvent object |
CLoggingEventHandler | An event handler for capturing the device logging event |
CPGMOption | Options for saving PGM images |
CPNGOption | Options for saving PNG images |
CPPMOption | Options for saving PPM images |
CSIOption | Options for saving Spinnaker image |
CSpinnakerGPU | Provides the functionality for the user to post process images on an NVIDIA GPU device |
CSystem | The system object is used to retrieve the list of interfaces and cameras available |
CSystemEventHandler | A handler to interface arrival and removal events on the system |
CSystemPtr | A reference tracked pointer to a system object |
CTIFFOption | Options for saving TIFF images |
CTransportLayerDevice | Part of the QuickSpin API to provide access to camera information without having to first initialize the camera |
CTransportLayerInterface | Part of the QuickSpin API to provide access to camera information without having to first initialize the camera |
CTransportLayerStream | Part of the QuickSpin API to provide access to camera information without having to first initialize the camera |
CTransportLayerSystem | Part of the QuickSpin API to provide access to camera information without having to first initialize the camera |