FLIR
Blackfly®S BFS-PGE-13Y3 |
Installing Your Blackfly S
1. Install the Tripod Mounting Bracket (optional)
![]() |
The ASA and ISO-compliant tripod mounting bracket attaches to the camera using the included screws. |
2. Attach a Lens
Unscrew the dust cap from the lens holder to install a lens.
3. Connect the interface Card and Cable to the Camera
![]() |
Plug the interface cable into the host controller card and the camera. The cable jack screws can be used for a secure connection. |
When the camera is first connected, the operating system automatically installs the camera driver. Camera drivers are available with the Spinnaker SDK installation.
- If using PoE, connect a powered Ethernet switch or Ethernet power injector in between the card and the camera.
4. Plug in the GPIO connector if required
![]() |
GPIO can be used for power, trigger, and strobe. |
5. Confirm Successful Installation
Run the SpinView application: Start->All Programs-> Point Grey Spinnaker->SpinView
The SpinView application can be used to test the camera's image acquisition capabilities.
Changes to your camera's installation configuration can be made using the SpinView application.
5/3/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
Blackfly®S BFS-PGE-13Y3 |
|