BFS-PGE-13Y3 Release Notes
Product Information
Product: BFS-PGE-13Y3
Firmware Version: 2111.0000.112.000
Bugs Fixed
| Bug |
Description |
| 53802 |
CRC was invalid for image sizes that were not 16 byte aligned |
| 54662 |
Offsets for serial port event data, length, and timestamp were incorrect in In camera XML |
| 54839 |
Camera sometimes does not acknowledge command before device reset |
| 55149 |
CRC position was incorrect for image sizes that were not a multiple of 4 bytes |
| 55508 |
GEV_STATUS_SUCCESS returned on unaligned writes |
| 55942 |
Framerate is 1 fps after Ethernet cable is disconnected/reconnected with external power |
| F-101 |
ARP failure with multiple hosts |
| F-327 |
Camera now always starts in PTP slave mode |
| F-362 |
PTP start-up delay set incorrectly |
| F-520 |
Nodes were not being updated when in auto mode. For auto algorithm features, changed Cachable to NoCache and added PollingTime of 500. |
| F-697 |
Camera sometimes does not acknowledge command before device reset |
| F-1081 |
Line1 (OptoOut) did not have an Off state |
| F-1532 |
Fixed duplicate EnumEntry values in GevSupportedOptionSelector node |
| F-3581 |
Persistent IP could fail if link is restored while camera is powered externally |
| F-4700 |
Allow persistent default gateway to be 0.0.0.0 |
| F-5071 |
Camera LED was solid green while acquisition not enabled. |
| F-5203 |
Pixel dynamic range max value was incorrect for 10-bit pixel formats |
| F-5204 |
When setting AcquisitionFrameRatePersistent to enabled, frame rate value in User Set was not being applied after power cycle. |
| F-6036 |
FIRM-6036 Reset receive FIFO when error occurs so that the command interface does not lock up. |
| F-6057 |
OffsetY was incorrect in GVSP Extended Chunk Data leader. |
| F-6587 |
When IP stack aborts, reboot camera instead of going into updater mode. |
| F-6730 |
FPGA and Firmware lose sync in the ethernet receive buffer under high packet traffic. |
Changes
| Change |
Description |
| 52286 |
Added ChunkExposureEndLineStatusAll feature to chunk data |
| 54819 |
Added support for 10-bit pixel formats |
| F-18 |
Added support for Action Commands |
| F-894 |
Added support for enabling GigEVision extended status codes |
| F-1082 |
Added ControlPacketsReservedBandwidth feature to control the reserved device link bandwidth for GVCP packets. |
| F-1600 |
Added UserSetFeature category |
| F-5156 |
Add LLC support |
Known Issues