FLIR
Blackfly®S BFS-PGE-23S3 |
Event Serial Port Receive Data
Category that contains all the data features related to the Serial Port Receive Event.
Summary Table
Name | Interface | Access | Visibility | Description |
---|---|---|---|---|
Event Serial Port Receive | IInteger | RO | Expert | Returns the unique identifier of the Serial Port Receive type of Event. |
Event Serial Port Receive Timestamp | IInteger | RO | Expert | Returns the Timestamp of the Serial Port Receive Event. |
Event Serial Data | IStringReg | Expert | Returns the serial data that was received. | |
Event Serial Data Length | IInteger | RO | Expert | Returns the length of the received serial data that was included in the event payload. |
Event Serial Receive Overflow | IBoolean | RO | Expert | Returns the status of the event serial receive overflow. |
Event Serial Port Receive Data Features
Event Serial Port Receive
Returns the unique identifier of the Serial Port Receive type of Event.
Property | Value |
---|---|
Name | EventSerialPortReceive |
Interface | IInteger |
Access | RO |
Unit | |
Visibility | Expert |
Value | 0x9C45 |
Event Serial Port Receive Timestamp
Returns the Timestamp of the Serial Port Receive Event.
Property | Value |
---|---|
Name | EventSerialPortReceiveTimestamp |
Interface | IInteger |
Access | RO |
Unit | |
Visibility | Expert |
Event Serial Data
Returns the serial data that was received.
Property | Value |
---|---|
Name | EventSerialData |
Interface | IStringReg |
Access | |
Visibility | Expert |
Event Serial Data Length
Returns the length of the received serial data that was included in the event payload.
Property | Value |
---|---|
Name | EventSerialDataLength |
Interface | IInteger |
Access | RO |
Unit | |
Visibility | Expert |
Event Serial Receive Overflow
Returns the status of the event serial receive overflow.
Property | Value |
---|---|
Name | EventSerialReceiveOverflow |
Interface | IBoolean |
Access | RO |
Visibility | Expert |
12/11/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
Blackfly®S BFS-PGE-23S3 |