Event Control
Event Features
Events allow you to get notified when the camera has performed something you might find interesting. Events are similar to the asynchronous communication but the difference is the initiator is the device.
Once an event is turned on, it has its own XML area where it outputs the event's ID, timestamp, and any applicable event data.
Use EventSelector to choose an event, then use EventNotification to set the event On or Off.
The possible events to choose are:
Exposure End - Event is sent every image when exposure end occurs. Event data includes: the event ID, timestamp, and frame ID.
Error - Event is sent every time an error occurs internally in the device. Event data includes: the event ID, timestamp, frame ID, and error code.
In order to verify that events are working, there is a TriggerEventTest command which allows you to trigger the camera to send a test event out.
Event Test - Event you can trigger to verify events are working properly. This is always enabled. Event data includes: exposure end ID and exposure end timestamp.
Summary Table
| Name | Interface | Access | Visibility | Description | 
|---|---|---|---|---|
| Event Selector | IEnumeration | RW | Expert | Selects which Event to enable or disable. | 
| Event Notification [Event Selector] | IEnumeration | RW | Expert | Enables/Disables the selected event. | 
| Event Exposure End Data | ICategory | RO | Expert | Category that contains all the data features related to the Exposure End Event. | 
| Event Error Data | ICategory | RO | Expert | Category that contains all the data features related to the Error Event. | 
| Event Serial Port Receive Data | ICategory | RO | Expert | Category that contains all the data features related to the Serial Port Receive Event. | 
| Event Test Data | ICategory | RO | Expert | Category that contains all the data features related to the Test Event. | 
Event Control Features
Event Selector
Selects which Event to enable or disable.
| Property | Value | 
|---|---|
| Name | EventSelector | 
| Interface | IEnumeration | 
| Access | RW | 
| Visibility | Expert | 
| Enumeration Values | 
|---|
| Error | 
| ExposureEnd | 
| SerialPortReceive | 
Event Notification
Enables/Disables the selected event.
| Property | Value | 
|---|---|
| Name | EventNotification [Event Selector] | 
| Interface | IEnumeration | 
| Access | RW | 
| Visibility | Expert | 
| Enumeration Values | 
|---|
| On | 
| Off | 
Event Exposure End Data
Category that contains all the data features related to the Exposure End Event.
| Property | Value | 
|---|---|
| Name | EventExposureEndData | 
| Interface | ICategory | 
| Access | RO | 
| Visibility | Expert | 
Event Error Data
Category that contains all the data features related to the Error Event.
| Property | Value | 
|---|---|
| Name | EventErrorData | 
| Interface | ICategory | 
| Access | RO | 
| Visibility | Expert | 
Event Serial Port Receive Data
Category that contains all the data features related to the Serial Port Receive Event.
| Property | Value | 
|---|---|
| Name | EventSerialPortReceiveData | 
| Interface | ICategory | 
| Access | RO | 
| Visibility | Expert | 
Event Test Data
Category that contains all the data features related to the Test Event.
| Property | Value | 
|---|---|
| Name | EventTestData | 
| Interface | ICategory | 
| Access | RO | 
| Visibility | Expert | 
_242x41.jpg)