You are here: Installation Guide > Physical Interface > Interface Connector
FLIR

Blackfly®S

BFS-PGE-27S5

 

Interface Connector

Ethernet Connector

The 8-pin RJ-45 Ethernet jack is equipped with two (2) M2 screwholes for secure connection. Pin assignments conform to the Ethernet standard.

Power over Ethernet (PoE)

To use PoE, an Ethernet power injector or a powered Ethernet switch must be connected to the camera. The PoE conforms to the IEEE 802.3af-2003 standard.

Pin Signal Name Description
1 VBUS Power
2 D- USB 2.0 differential pair
3 D+
4 ID OTG identification
5 GND Ground for power return
6 MicB_SSTX- SuperSpeed transmitter differential pair
7 MicB_SSTX+
8 GND_DRAIN Ground for SuperSpeed signal return
9 MicB_SSRX- SuperSpeed receiver differential pair
10 MicB_SSRX+

 

9/13/2019
© 2015-2019 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-PGE-27S5
Camera Reference