Event Exposure End Data
Category that contains all the data features related to the Exposure End Event.
Summary Table
| Name | Interface | Access | Visibility | Description |
|---|---|---|---|---|
| Event Exposure End | IInteger | RO | Expert | Returns the unique identifier of the Exposure End type of Event. |
| Event Exposure End Timestamp | IInteger | RO | Expert | Returns the Timestamp of the Exposure End Event. |
| Event Exposure End Frame ID | IInteger | RO | Expert | Returns the unique Identifier of the Frame (or image) that generated the Exposure End Event. |
Event Exposure End Data Features
Event Exposure End
Returns the unique identifier of the Exposure End type of Event.
| Property | Value |
|---|---|
| Name | EventExposureEnd |
| Interface | IInteger |
| Access | RO |
| Unit | |
| Visibility | Expert |
| Value | 0x9C43 |
Event Exposure End Timestamp
Returns the Timestamp of the Exposure End Event.
| Property | Value |
|---|---|
| Name | EventExposureEndTimestamp |
| Interface | IInteger |
| Access | RO |
| Unit | |
| Visibility | Expert |
Event Exposure End Frame ID
Returns the unique Identifier of the Frame (or image) that generated the Exposure End Event.
| Property | Value |
|---|---|
| Name | EventExposureEndFrameID |
| Interface | IInteger |
| Access | RO |
| Unit | |
| Visibility | Expert |
_242x41.jpg)