Serial Port Control
                                        
                                        Serial Port
                                        The serial port can be used to transmit and receive serial data through the 
device using the transport layer. The serial data can be sent through the 
transport layer in image data (via the SerialData Chunk Data), in control data 
(via the File Access Control), or in event data (via the SerialPortReceive Event).
                                        The serial port to configure is selected using the 
SerialPortSelector. The physical line on which 
to receive serial data is set using the SerialPortSource. 
The physical line on which to transmit serial data is set using the LineSource 
in the Digital IO Control. The serial port settings for both the receive and 
transmit can be set using the SerialPortBaudRate, 
SerialPortDataBits, 
SerialPortStopBits¸ and
SerialPortParity.
                                        Serial data can be transmitted and received through the File Access Control. 
Once the serial port file is opened, data can be transmitted via Write operations 
and received via Read operations. Received serial data can also be obtained through 
the SerialPortReceive Event which will be generated when data is available or 
through the SerialData Chunk Data which is appended into each image payload.
                                        The total number of characters in the serial port transmit and receive queues 
can be monitored using the 
SerialTransmitQueueMaxCharacterCount 
and the SerialReceiveQueueMaxCharacterCount. 
The current number of characters in the queues can be monitored using the 
SerialTransmitQueueCurrentCharacterCount 
and SerialReceiveQueueCurrentCharacterCount. 
The SerialReceiveQueueCurrentCharacterCount 
reports the maximum number of characters that can be obtained using the File Access Control. 
The receive queue can be emptied by executing the 
SerialReceiveQueueClear.
                                        Serial port framing and parity errors are reported using the 
SerialRecieveFramingErrorCount and the 
SerialReceiveParityErrorCount. Overflow 
errors are reported within the SerialData Chunk Data, the SerialPortReceive Event, 
or in the FileOperationStatus after executing a Read.
                                        Summary Table
                                        
                                        
                                         Serial Port Control Features 
                                        
                                         Serial Port Selector
                                        Selects which serial port of the device to control.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialPortSelector
                     | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IEnumeration | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RW | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                        
                                            
                                                
                                                    | Enumeration Values | 
                                                
                                            
                                            
                                                
                                                    | SerialPort0
                                                     | 
                                                
                                            
                                        
                                        
                                         Serial Port Source
                                        Specifies the physical input Line on which to receive serial data.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialPortSource
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IEnumeration | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RW | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                        
                                            
                                                
                                                    | Enumeration Values | 
                                                
                                            
                                            
                                                
                                                    | Line0
                                                     | 
                                                
                                                
                                                    | Line1
                                                     | 
                                                
                                                
                                                    | Line2
                                                     | 
                                                
                                                
                                                    | Line3
                                                     | 
                                                
                                                
                                                    | Off
                                                     | 
                                                
                                            
                                        
                                        
                                         Serial Port Baud Rate
                                        This feature controls the baud rate used by the selected serial port.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialPortBaudRate
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IEnumeration | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RW | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                        
                                            
                                                
                                                    | Enumeration Values | 
                                                
                                            
                                            
                                                
                                                    | Baud300
                                                     | 
                                                
                                                
                                                    | Baud600
                                                     | 
                                                
                                                
                                                    | Baud1200
                                                     | 
                                                
                                                
                                                    | Baud2400
                                                     | 
                                                
                                                
                                                    | Baud4800
                                                     | 
                                                
                                                
                                                    | Baud9600
                                                     | 
                                                
                                                
                                                    | Baud14400
                                                     | 
                                                
                                                
                                                    | Baud19200
                                                     | 
                                                
                                                
                                                    | Baud38400
                                                     | 
                                                
                                                
                                                    | Baud57600
                                                     | 
                                                
                                                
                                                    | Baud115200
                                                     | 
                                                
                                            
                                        
                                        
                                         Serial Port Data Bits
                                        This feature controls the number of data bits used by the selected serial port. Possible values that can be used are between 5 and 9.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialPortDataBits
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RW | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Serial Port Stop Bits
                                        This feature controls the number of stop bits used by the selected serial port.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialPortStopBits
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IEnumeration | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RW | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                        
                                            
                                                
                                                    | Enumeration Values | 
                                                
                                            
                                            
                                                
                                                    | Bits1
                                                     | 
                                                
                                                
                                                    | Bits1AndAHalf
                                                     | 
                                                
                                                
                                                    | Bits2
                                                     | 
                                                
                                            
                                        
                                        
                                         Serial Port Parity
                                        This feature controls the parity used by the selected serial port.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialPortParity
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IEnumeration | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RW | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                        
                                            
                                                
                                                    | Enumeration Values | 
                                                
                                            
                                            
                                                
                                                    | None
                                                     | 
                                                
                                                
                                                    | Odd
                                                     | 
                                                
                                                
                                                    | Even
                                                     | 
                                                
                                                
                                                    | Mark
                                                     | 
                                                
                                                
                                                    | Space
                                                     | 
                                                
                                            
                                        
                                        
                                         Transmit Queue Max Character Count
                                        >Returns the maximum number of characters in the serial port transmit queue.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialTransmitQueueMaxCharacterCount
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RO | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Transmit Queue Current Character Count
                                        Returns the number of characters currently in the serial port transmit queue.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialTransmitQueueCurrentCharacterCount
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RO | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Receive Queue Max Character Count
                                        >Returns the maximum number of characters in the serial port receive queue.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialReceiveQueueMaxCharacterCount
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RO | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Receive Queue Current Character Count
                                        Returns the number of characters currently in the serial port receive queue.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialReceiveQueueCurrentCharacterCount
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RO | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Receive Queue Clear
                                        This is a command that clears the device serial port receive queue.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialReceiveQueueClear
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    ICommand | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    WO | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Receive Framing Error Count
                                        Returns the number of framing errors that have occurred on the serial port.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialReceiveFramingErrorCount
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RO | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert | 
                                                
                                            
                                        
                                        
                                         Receive Parity Error Count
                                        Returns the number of parity errors that have occurred on the serial port.
                                        
                                            
                                                
                                                    | Property | 
                                                    Value | 
                                                
                                            
                                            
                                                
                                                    | Name
                                                     | 
                                                    SerialReceiveParityErrorCount
                    [Serial Port Selector] | 
                                                
                                                
                                                    | Interface
                                                     | 
                                                    IInteger | 
                                                
                                                
                                                    | Access
                                                     | 
                                                    RO | 
                                                
                                                
                                                    | Unit
                                                     | 
                                                     | 
                                                
                                                
                                                    | Visibility
                                                     | 
                                                    Expert |