Installing your Interface Card and Software

1. Install your Interface Card

 

Ensure the card is installed per the manufacturer's instructions.

Connect the internal IDE or SATA power connector on the card to the computer power supply.

Alternatively, use your PC's built-in host controller, if equipped.

Open the Windows Device Manager. Ensure the card is properly installed. Ethernet cards appear under Network Adapters. An exclamation point (!) next to the card indicates the driver has not yet been installed.

2. Install the Spinnaker® SDK Software

Note: For existing users who already have Spinnaker installed, we recommend ensuring you have the latest version for optimal performance of your camera. If you do not need to install Spinnaker, use SpinView to install and enable drivers for your card.
  1. Go to the Spinnaker SDK page.
  2. Click the Download button. You are prompted to login, if not already.
  3. Select your operating system. Depending on your selection there may be other versions to select.
  4. After download is complete, open the file to start the Spinnaker setup wizard.
  5. Follow the steps in each setup dialog.

3. For GigE cameras—Enable jumbo frames on the Ethernet card

  1. In StartÒAll ProgramsÒSpinnaker SDKÒSpinView, right click on the Network Adapter and select Adapter Configuration, then select IP Configuration.
  2. Click Open Network Connections.
  3. Click Change Settings.
  4. Click on the Advanced tab and from the Settings list select Jumbo Packet.
  5. Set the Value to 9014 Bytes and click OK.

See How to Optimize GigE Network Adapter Settings for more information on configuring for best performance.