Transport Layer Control

The Transport Layer control provides the following information:

Gev IEEE 1588 - Enables IEEE 1588 Precision Time Protocol (PTP) to control the timestamp register.

Gev IEEE 1588 Clock Accuracy - The expected accuracy of the device clock when it is the grandmaster or when it becomes the grandmaster.

Gev IEEE 1588 Status - The status of the IEEE 1588 clock.

Gev IEEE 1588 Mode - The mode of the IEEE 1588 clock.

Summary Table

Name Interface Access Visibility Description
Payload Size IInteger Expert Provides the number of bytes transferred for each image or chunk on the stream channel.
GigE Vision ICategory RO Beginner Category that contains the features pertaining to the GigE Vision transport layer of the device.
Link Error Count IInteger RO Expert Counts the number of error on the link.
Packet Resend Request Count IInteger RO Expert Counts the number of resend requests received from the host.

Transport Layer Control Features


Payload Size

Provides the number of bytes transferred for each image or chunk on the stream channel.

Property Value
Name PayloadSize
Interface IInteger
Access
Unit
Visibility Expert

GigE Vision

Category that contains the features pertaining to the GigE Vision transport layer of device, including IEEE 1588.

Property Value
Name GigEVision
Interface ICategory
Access RO
Visibility Beginner

Link Error Count

Counts the number of error on the link.

Property Value
Name LinkErrorCount
Interface IInteger
Access RO
Unit
Visibility Expert

Packet Resend Request Count

Counts the number of resend requests received from the host.

Property Value
Name PacketResendRequestCount
Interface IInteger
Access RO
Unit
Visibility Expert