Transport Layer Control
The Transport Layer control provides the following information:
Gev IEEE 1588 - Enables IEEE 1588 Precision Time Protocol (PTP) to control the timestamp register.
Gev IEEE 1588 Clock Accuracy - The expected accuracy of the device clock when it is the grandmaster or when it becomes the grandmaster.
Gev IEEE 1588 Status - The status of the IEEE 1588 clock.
Gev IEEE 1588 Mode - The mode of the IEEE 1588 clock.
Summary Table
| Name | Interface | Access | Visibility | Description | 
|---|---|---|---|---|
| Payload Size | IInteger | Expert | Provides the number of bytes transferred for each image or chunk on the stream channel. | |
| GigE Vision | ICategory | RO | Beginner | Category that contains the features pertaining to the GigE Vision transport layer of the device. | 
| Link Error Count | IInteger | RO | Expert | Counts the number of error on the link. | 
| Packet Resend Request Count | IInteger | RO | Expert | Counts the number of resend requests received from the host. | 
Transport Layer Control Features
Payload Size
Provides the number of bytes transferred for each image or chunk on the stream channel.
| Property | Value | 
|---|---|
| Name | PayloadSize | 
| Interface | IInteger | 
| Access | |
| Unit | |
| Visibility | Expert | 
GigE Vision
Category that contains the features pertaining to the GigE Vision transport layer of device, including IEEE 1588.
| Property | Value | 
|---|---|
| Name | GigEVision | 
| Interface | ICategory | 
| Access | RO | 
| Visibility | Beginner | 
Link Error Count
Counts the number of error on the link.
| Property | Value | 
|---|---|
| Name | LinkErrorCount | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
Packet Resend Request Count
Counts the number of resend requests received from the host.
| Property | Value | 
|---|---|
| Name | PacketResendRequestCount | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
_242x41.jpg)