You are here: Installation Guide > Physical Interface > Mounting with the Case or Mounting Bracket
FLIR

Blackfly®S

BFS-U3-04S2

 

Mounting with the Case or Mounting Bracket

Using the Case

The case is equipped with the following mounting holes:

  • Two (2) M2 x 2mm mounting holes on the top of the case
  • Three (3) M3 x 2.5mm mounting holes on the bottom of the case
  • Four (4) M2 x 2mm mounting holes on the bottom of the case that can be used to attach the camera directly to a custom mount or to the tripod mounting bracket

Using the Mounting Bracket

The tripod mounting bracket is equipped with four (4) M2 mounting holes.

Tripod Adapter Dimensions

Tripod Adapter Dimensional Diagram

 

11/15/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-04S2
Camera Reference

FLIR Camera and API References