FLIR

Blackfly®S

BFS-U3-04S2

 

Signal to Noise Ratio

This test measures the ratio of the maximum signal produced by the device to the noise level. The measurement is made in decibels (dB).

Pass/Fail Criteria

All measurements must meet or exceed TBDTBD.

Test Stages and Configurations

Test Stage Test Configuration
U4 ETC I, STC I
U6 ETC I, STC I

 

Additional Configuration

  • Gain is set to 0 dB.
  • Black level is set high enough not to truncate the noise.

 

11/15/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-04S2
Camera Reference

FLIR Camera and API References