You are here: Quality > Unit Tests > Data Storage
FLIR

Blackfly®S

BFS-U3-120S4

 

Data Storage

This test ensures that the device's on-board user data storage is accessible and functions correctly. This is done through a series of reads and writes to the entire storage space. Data is written to the device and then confirmed on read.

Pass/Fail Criteria

  • 100% of the reads and writes across the entire storage space must be successful.

Test Stages and Configurations

Test Stage Test Configuration
U6 STC I

 

Additional Configuration

  • Test is run while the device is not streaming.

 

5/4/2018
© 2015-2017 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-120S4
Camera Reference

FLIR Camera and API References