BFS-U3-122S6 Release Notes
Product Information
Product: BFS-U3-122S6
Firmware Version: 2309.0000.533.000
Bugs Fixed
| Bug |
Description |
| F-1082 |
Transfer Queue Overflow can occur when streaming at max frame rate in auto acquisition frame rate mode |
| F-520 |
Nodes are not being updated when in auto mode on BFS |
| F-1081 |
Line1 (OptoOut) does not have an Off state |
| F-4114 |
Camera could fail due to packet resend |
| F-2611 |
"Packet Resend Request Count" is set to linear (slider) instead of PureNumber |
| F-4004 |
Camera starts up at 1fps after PC power cycles with camera connected |
| F-4700 |
SpinView cannot set Persistent IP for BFS cameras when Default Gateway is set to 0.0.0.0 |
| F-5203 |
Pixel dynamic range max value incorrect for 10-bit pixel formats |
| F-5204 |
When setting AcquisitionFrameRatePersistent to enabled, frame rate value in User Set was not being applied after power cycle |
| F-5071 |
Camera LED was solid green while acquisition not enabled |
| F-5310 |
Bayer pattern changes are not picked up if ISP is off |
| F-7404 |
Chunk serial data is misaligned |
Changes
| Change |
Description |
| F-5156 |
Added Lossless Compression (LLC) feature |
| F-9850 |
Added Lens Shading Correction (LSC) feature |
Known Issues