FLIR
Blackfly®S BFS-U3-13Y3 |
Lens Mounting
Lenses are not included with individual cameras.
Title | Article |
---|---|
Selecting a lens for your camera | Knowledge Base Article 10694 |
The lens mount is compatible with C-mount lenses. Correct focus cannot be achieved using a CS-mount lens on a C-mount camera.
Example C-mount Cross Section
Back Flange Distance
The Back Flange Distance (BFD) is offset due to the presence of both a 1 mm infrared cutoff (IRC) filter and a 0.5 mm sensor package window. These two pieces of glass fit between the lens and the sensor image plane. The IRC filter is installed on color cameras. In monochrome cameras, it is a transparent piece of glass. The sensor package window is installed by the sensor manufacturer. Both components cause refraction, which requires some offset in flange back distance to correct.
The resulting C-mount BFD is 17.99 mm.
For more information about the IRC filter, see Infrared Cut-Off Filters.
2/2/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
Blackfly®S BFS-U3-13Y3 |
|