FLIR
Blackfly®S BFS-U3-13Y3 |
Transport Layer Control
The Transport Layer control provides the following information:
Payload Size - the number of bytes transferred for each image (including chunk data).
USB3 Vision Tab - Message Channel - Channel ID used for the Message Channel.
U3v Version Major/Minor - USB3 Vision standard version.
U3V Capabilities - what the camera supports (SIRM, EIRM and IIDC2).
Max Command Transfer Length - the maximum supported commands that can be sent to the camera.
Max Ack Transfer Length - the maximum supported ack that can be sent to the camera.
Number of Stream Channels - the number of stream channels the camera supports.
Current Speed - the speed of the camera's interface (Super Speed, High Speed).
Link Error Count - the number of errors on the usb link.
Link Recovery Count - the number of times the USB link has recovered.
Summary Table
Name | Interface | Access | Visibility | Description |
---|---|---|---|---|
Payload Size | IInteger | Expert | Provides the number of bytes transferred for each image or chunk on the stream channel. | |
USB3 Vision | ICategory | RO | Beginner | Category that contains the features pertaining to the USB3 Vision transport layer of the device. |
Link Error Count | IInteger | RO | Expert | Counts the number of error on the link. |
Link Recovery Count | IInteger | RO | Expert | Counts the number of times the USB link has recovered. |
Transport Layer Control Features
Payload Size
Provides the number of bytes transferred for each image or chunk on the stream channel.
Property | Value |
---|---|
Name | PayloadSize |
Interface | IInteger |
Access | |
Unit | |
Visibility | Expert |
USB3 Vision
Category that contains the features pertaining to the USB3 Vision transport layer of the device.
Property | Value |
---|---|
Name | USB3Vision |
Interface | ICategory |
Access | RO |
Visibility | Beginner |
Link Error Count
Counts the number of error on the link.
Property | Value |
---|---|
Name | LinkErrorCount |
Interface | IInteger |
Access | RO |
Unit | |
Visibility | Expert |
Link Recovery Count
Counts the number of times the USB link has recovered.
Property | Value |
---|---|
Name | LinkRecoveryCount |
Interface | IInteger |
Access | RO |
Unit | |
Visibility | Expert |
2/2/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
Blackfly®S BFS-U3-13Y3 |
|