You are here: Quality > Unit Tests > Enumeration
FLIR

Blackfly®S

BFS-U3-13Y3

 

Enumeration

This test confirms that the device consistently powers up and is enumerated by the host device. This is done through a programmed series of power cycles and device enumerations.

Pass/Fail Criteria

  • The device must correctly enumerate 100% of the time.

Test Stages and Configurations

Test Stage Test Configuration
U6 STC I

 

Additional Configuration

  • None.

 

2/2/2017
© 2015-2017 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.

Legal
| Contact Support

Blackfly®S BFS-U3-13Y3
Camera Reference