Interface Cables
To purchase a recommended cable from Teledyne FLIR, visit the Products Accessories page.
Category 5e or 6 cables up to 100 meters in length should be used for connecting the camera to the network interface card on the host system. Teledyne FLIR sells a 5-meter Category 5e cable for this purpose.
Note: For optimal ESD protection, we recommend using a shielded Ethernet
cable or connecting the camera housing to chassis ground (earth).
The USB3 standard does not specify a maximum cable length. FLIR sells a number of cable options. Visit the Product Accessories page for more information.
Note: A 5-meter USB3 cable (or longer) is not recommended for laptops or on board controllers.
| Extending the Working Distance of USB3 Cameras |
_242x41.jpg)