Installing Your Blackfly S
1. Prepare the lens mount.
![]() |
The board-level models can use C-mounts, CS-mounts, or S-mounts. For C- and CS-mounts, install the retainer, flip over and place IR filter in it then install the gasket. |
2. Remove sticker and install lens mount.
![]() |
The sensor is covered with a protective sticker. Remove the sticker. If any residue is present, clean the sensor surface with a non-abrasive cotton swab and isopropyl alcohol cleaning solution. Immediately install the image board over the prepared lens mount. |
3. Install a heat sink.
![]() |
A heatsink (ACC-01-7000) is recommended but depends on your design and usage. |
4. Connect the FPC cable to the panel mount adapter then connect the adapter to the interface card.
![]() |
|
5. Attach a Lens
6. Plug in the GPIO connector if required
GPIO can be used for trigger, serial input output, and strobe.
7. Confirm Successful Installation
When the camera is first connected, the operating system automatically installs the camera driver. Camera drivers are available with the Spinnaker SDK installation.
Run the SpinView application: Start->All Programs->Spinnaker->SpinView
The SpinView application can be used to test the camera's image acquisition capabilities.
Changes to your camera's installation configuration can be made using the SpinView application.