You are here: Installation Guide > Physical Interface > Lens Mounting
FLIR

Blackfly®S

BFS-U3-23S3

 

Lens Mounting

Lenses are not included with the cased model cameras.

Related Knowledge Base Articles
Title Article
Selecting a lens for your camera Knowledge Base Article 10694

 

C-mount models CS-mount models
BFS-PGE-13Y3 / BFS-U3-13Y3 BFS-PGE-04S2 / BFS-U3-04S2
BFS-PGE-31S4 / BFS-U3-31S4 BFS-PGE-16S2 / BFS-U3-16S2
BFS-PGE-23S3 / BFS-U3-23S3 BFS-U3-120S4
BFS-U3-32S4  
BFS-PGE-50S5 / BFS-U3-50S5  
BFS-PGE-51S5 / BFS-U3-51S5  
BFS-U3-63S4  
BFS-PGE-88S6 / BFS-U3-88S6  
BFS-U3-89S6  
BFS-PGE-122S6 / BFS-U3-122S6  
BFS-U3-123S6  
BFS-PGE-200S6 / BFS-U3-200S6  

 

Correct focus cannot be achieved using a CS-mount lens on a C-mount camera.

Example C-mount Cross Section

Back Flange Distance

The Back Flange Distance (BFD) is offset due to the presence of both a 1 mm infrared cutoff (IRC) filter and a 0.5 mm sensor package window. These two pieces of glass fit between the lens and the sensor image plane. The IRC filter is installed on color cameras. In monochrome cameras, it is a transparent piece of glass. The sensor package window is installed by the sensor manufacturer. Both components cause refraction, which requires some offset in flange back distance to correct.

The resulting C-mount BFD is 17.99 mm.

The resulting CS-mount BFD is 12.52 mm.

For more information about the IRC filter, see Infrared Cut-Off Filters.

 

12/6/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-23S3
Camera Reference

FLIR Camera and API References