FLIR
Blackfly®S BFS-U3-31S4-BD |
Data Storage
This test ensures that the device's on-board user data storage is accessible and functions correctly. This is done through a series of reads and writes to the entire storage space. Data is written to the device and then confirmed on read.
Pass/Fail Criteria
- 100% of the reads and writes across the entire storage space must be successful.
Test Stages and Configurations
Test Stage | Test Configuration |
---|---|
U6 | STC I |
Additional Configuration
- Test is run while the device is not streaming.
2/11/2020
© 2015-2020 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
|