You are here: Installation Guide > Configuring Camera Setup > Configuring Camera Drivers
FLIR

Blackfly®S

BFS-U3-31S4

 

Configuring Camera Drivers

Camera drivers are provided as part of the Spinnaker SDK. The first time the camera is connected to the computer, the operating system installs the driver.

To manage and update drivers use the SpinView application:

  1. Start SpinView:
  2. Start Menu-->All Programs-->Point Grey Spinnaker SDK-->SpinView
  3. From the Devices list, select the camera and click the Switch Driver button.
  4. Select the driver from the drop-down list.
  5. Click Install Driver.

 

5/30/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-31S4
Camera Reference

FLIR Camera and API References