FLIR
Blackfly®S BFS-U3-50S5-BD2 |
Interface Card
To purchase a compatible card from FLIR, visit the Products Accessories page.
The camera must connect to an interface card. This is sometimes called a host adapter, a bus controller, or a network interface card (NIC).
In order to achieve the maximum benefits of USB3, the camera must connect to a USB3 PCIe 2.0 card. The card must be connected to the PC power supply in order to power the camera through the USB3 interface.
6/28/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
Blackfly®S BFS-U3-50S5-BD2 |