You are here: Installation Guide > Camera Installation > Installing Your Camera
FLIR

Blackfly®S

BFS-U3-50S5-BD2

 

Installing Your Blackfly S

1. Install the lens mount.

The board-level models can use C-mounts, CS-mounts, or S-mounts.

 

2. Install a heat sink.

A heatsink is recommended but depends on your design and usage.

3. Connect the FPC cable to the panel mount adapter then connect the adapter to the interface card.

A TF38 to FPC USB3 panel mount adapter allows a USB3 cable connection to a PC.

4. Attach a Lens

5. Plug in the GPIO connector if required

GPIO can be used for power, trigger, serial input output, and strobe.

6. Confirm Successful Installation

When the camera is first connected, the operating system automatically installs the camera driver. Camera drivers are available with the Spinnaker SDK installation.

Run the SpinView application: Start->All Programs-> Point Grey Spinnaker->SpinView
The SpinView application can be used to test the camera's image acquisition capabilities.

Changes to your camera's installation configuration can be made using the SpinView application.

 

6/28/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-50S5-BD2
Camera Reference

FLIR Camera and API References