Event Serial Port Receive Data
Category that contains all the data features related to the Serial Port Receive Event.
Summary Table
| Name | Interface | Access | Visibility | Description | 
|---|---|---|---|---|
| Event Serial Port Receive | IInteger | RO | Expert | Returns the unique identifier of the Serial Port Receive type of Event. | 
| Event Serial Port Receive Timestamp | IInteger | RO | Expert | Returns the Timestamp of the Serial Port Receive Event. | 
| Event Serial Data | IStringReg | Expert | Returns the serial data that was received. | |
| Event Serial Data Length | IInteger | RO | Expert | Returns the length of the received serial data that was included in the event payload. | 
| Event Serial Receive Overflow | IBoolean | RO | Expert | Returns the status of the event serial receive overflow. | 
Event Serial Port Receive Data Features
Event Serial Port Receive
Returns the unique identifier of the Serial Port Receive type of Event.
| Property | Value | 
|---|---|
| Name | EventSerialPortReceive | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
| Value | 0x9C45 | 
Event Serial Port Receive Timestamp
Returns the Timestamp of the Serial Port Receive Event.
| Property | Value | 
|---|---|
| Name | EventSerialPortReceiveTimestamp | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
Event Serial Data
Returns the serial data that was received.
| Property | Value | 
|---|---|
| Name | EventSerialData | 
| Interface | IStringReg | 
| Access | |
| Visibility | Expert | 
Event Serial Data Length
Returns the length of the received serial data that was included in the event payload.
| Property | Value | 
|---|---|
| Name | EventSerialDataLength | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
Event Serial Receive Overflow
Returns the status of the event serial receive overflow.
| Property | Value | 
|---|---|
| Name | EventSerialReceiveOverflow | 
| Interface | IBoolean | 
| Access | RO | 
| Visibility | Expert | 
_242x41.jpg)