FLIR
Blackfly®S BFS-U3-50S5 |
Installing Your Blackfly S
1. Install the Tripod Mounting Bracket (optional)
![]() |
The ASA and ISO-compliant tripod mounting bracket attaches to the camera using the included screws. |
2. Attach a Lens
Unscrew the dust cap from the lens holder to install a lens.
3. Connect the interface Card and Cable to the Camera
![]() |
Plug the interface cable into the host controller card and the camera. The cable jack screws can be used for a secure connection. |
When the camera is first connected, the operating system automatically installs the camera driver. Camera drivers are available with the Spinnaker SDK installation.
4. Plug in the GPIO connector if required
![]() |
GPIO can be used for power, trigger, and strobe. |
5. Confirm Successful Installation
Run the SpinView application: Start->All Programs-> Point Grey Spinnaker->SpinView
The SpinView application can be used to test the camera's image acquisition capabilities.
Changes to your camera's installation configuration can be made using the SpinView application.
6/8/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc. All rights reserved. Legal | Contact Support |
Blackfly®S BFS-U3-50S5 |