BFS-U3-50S5 Release Notes
Product Information
Product: BFS-U3-50S5
Firmware Version: 2308.0000.758.000
Bugs Fixed
| Bug |
Description |
| F-0520 |
Nodes are not being updated when in auto mode on BFS |
| F-1081 |
Line1 (OptoOut) does not have an Off state |
| F-1543 |
Added support for sensors which require longer per-frame write time |
| F-1893 |
Minimum exposure time now includes exposure time offset of the sensor |
| F-1657 |
Maximum Acknowledge should be 512 to avoid BSOD occurring in 3rd party library |
| F-3431 |
Sensor communication period has been extended |
| F-4504 |
Added USB image burst transmission support |
| F-4379 |
Upon PC reboot, camera would enumerate as USB2 or USB3 with USB2 link throughput limit |
| F-5203 |
Pixel dynamic range max value was incorrect for 10-bit pixel formats |
| F-5204 |
When setting AcquisitionFrameRatePersistent to enabled, frame rate value in User Set was not being applied after power cycle |
| F-5071 |
Camera LED was solid green while acquisition not enabled |
| F-5774 |
PC automatically reboot when camera finishing acquisition |
| F-5310 |
Bayer Sampling Module - Bayer pattern changes are not picked up if ISP is off |
| F-7895 |
BFS cameras have reliability issues on USB3 Fresco FL1100 card |
Changes
| Change |
Description |
| F-9960 |
Added Lens Shading Correction (LSC) feature |
Known Issues