You are here: Installation Guide > Physical Interface > Interface Card
FLIR

Blackfly®S

BFS-U3-63S4

 

Interface Card

To purchase a compatible card from FLIR, visit the Products Accessories page.

The camera must connect to an interface card. This is sometimes called a host adapter, a bus controller, or a network interface card (NIC).

In order to achieve the maximum benefits of USB 3.0, the camera must connect to a USB 3.0 PCIe 2.0 card. The card must be connected to the PC power supply in order to power the camera through the USB 3.0 interface.

 

5/4/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-63S4
Camera Reference

FLIR Camera and API References