You are here: Quality > Unit Tests > Enumeration
FLIR

Blackfly®S

BFS-U3-63S4

 

Enumeration

This test confirms that the device consistently powers up and is enumerated by the host device. This is done through a programmed series of power cycles and device enumerations.

Pass/Fail Criteria

  • The device must correctly enumerate 100% of the time.

Test Stages and Configurations

Test Stage Test Configuration
U6 STC I

 

Additional Configuration

  • None.

 

5/4/2018
© 2015-2018 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-63S4
Camera Reference

FLIR Camera and API References