You are here: Technical Reference > Event Control > Event Serial Port Receive Data
FLIR

Blackfly®S

BFS-U3-88S6-BD

 

Event Serial Port Receive Data

Category that contains all the data features related to the Serial Port Receive Event.

Summary Table

Name Interface Access Visibility Description
Event Serial Port Receive IInteger RO Expert Returns the unique identifier of the Serial Port Receive type of Event.
Event Serial Port Receive Timestamp IInteger RO Expert Returns the Timestamp of the Serial Port Receive Event.
Event Serial Data IStringReg Expert Returns the serial data that was received.
Event Serial Data Length IInteger RO Expert Returns the length of the received serial data that was included in the event payload.
Event Serial Receive Overflow IBoolean RO Expert Returns the status of the event serial receive overflow.

Event Serial Port Receive Data Features


Event Serial Port Receive

Returns the unique identifier of the Serial Port Receive type of Event.

Property Value
Name EventSerialPortReceive
Interface IInteger
Access RO
Unit
Visibility Expert
Value 0x9C45

Event Serial Port Receive Timestamp

Returns the Timestamp of the Serial Port Receive Event.

Property Value
Name EventSerialPortReceiveTimestamp
Interface IInteger
Access RO
Unit
Visibility Expert

Event Serial Data

Returns the serial data that was received.

Property Value
Name EventSerialData
Interface IStringReg
Access
Visibility Expert

Event Serial Data Length

Returns the length of the received serial data that was included in the event payload.

Property Value
Name EventSerialDataLength
Interface IInteger
Access RO
Unit
Visibility Expert

Event Serial Receive Overflow

Returns the status of the event serial receive overflow.

Property Value
Name EventSerialReceiveOverflow
Interface IBoolean
Access RO
Visibility Expert

 

2/11/2020
© 2015-2020 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Blackfly®S BFS-U3-88S6-BD
Camera Reference