FFY-U3-04S2 Release Notes
Product Information
Product: FFY-U3-04S2
Firmware Version: 2101.000.019.000
Bugs Fixed
| Bug | Description |
|---|---|
| F-380 | Toggling FrameStart TriggerMode on/off while acquisition is active distorts the transmitted images. |
| F-949 | FileSize node sometimes not updated to correct value if a file is overwritten. |
| F-1146 | New exposure time setting takes an extra frame to take effect in trigger mode. |
| F-4583 | Default trigger selector must be FrameStart. |
| F-4585 | Serial number sometimes becomes '0' when USB interface is disconnected/reconnected. |
Changes
| Change | Description |
|---|---|
| [1] | FFY-U3-04S2C initial firmware release for manufacturing mass production. |
| [2] | FFY-U3-04S2M firmware update. |
Known Issues
| Issue | Description |
|---|---|
| F-542 | Rapidly starting/stopping acquisition while using U3V events may make camera not responsive. |
| F-587 | U1 and U2 USB power states are advertised but do not work. |
| F-594 | Doing a firmware update may not work on some USB2 interfaces. |
| F-601 | USB device location node is incorrect. |
| F-991 | Spurious small voltage spikes can be observed on digital IO line 0 during state transitions. |
| F-1042 | There is a small (less than 1%) chance that camera will not re-enumerate after DeviceReset command is issued. |
_242x41.jpg)