Event Exposure End Data
Category that contains all the data features related to the Exposure End Event.
Summary Table
| Name | Interface | Access | Visibility | Description | 
|---|---|---|---|---|
| Event Exposure End | IInteger | RO | Expert | Returns the unique identifier of the Exposure End type of Event. | 
| Event Exposure End Timestamp | IInteger | RO | Expert | Returns the Timestamp of the Exposure End Event. | 
| Event Exposure End Frame ID | IInteger | RO | Expert | Returns the unique identifier of the frame (or image) that generated the Exposure End Event. | 
Event Exposure End Data Features
Event Exposure End
Returns the unique identifier of the Exposure End type of Event.
| Property | Value | 
|---|---|
| Name | EventExposureEnd | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
| Value | 0x9C43 | 
Event Exposure End Timestamp
Returns the Timestamp of the Exposure End Event.
| Property | Value | 
|---|---|
| Name | EventExposureEndTimestamp | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
Event Exposure End Frame ID
Returns the unique identifier of the frame (or image) that generated the Exposure End Event.
| Property | Value | 
|---|---|
| Name | EventExposureEndFrameID | 
| Interface | IInteger | 
| Access | RO | 
| Unit | |
| Visibility | Expert | 
_242x41.jpg)