| Bug |
Description |
| F-5455 |
Multi-frame acquisition mode may not always work when exposure is longer than readout time. |
| F-380 |
Toggling Frame Start Trigger Mode on/off while acquisition is active cause garbled output. |
| F-4583 |
TriggerSelector defaults to AcquisitionStart instead of FrameStart. |
| F-1088 |
AcquisitionStop USB flushing behaviour is incorrect. |
| F-937 |
No validation of CNN input/output size. |
| F-851 |
Colour camera inference unstable when using MONO8. |
| F-930 |
LUT constantly loading from device. |
| F-1046 |
Replace FP16 LUT with a proper pass-through LUT. |
| F-1146 |
Change in exposure time takes one extra frame to take effect in trigger mode. |
| F-957 |
Improve the execution efficiency and correctness of LUT update. |
| F-1022 |
Colour pixel formats missing from documentation. |
| F-4681 |
Cannot perform colour detection. |
| F-4843 |
Streaming freezes when done with inference for an extended period of time. |
| F-993 |
Inference related nodes are not saved to userset. |
| F-5456 |
IMX296 max framerate is incorrect. |
| F-5662 |
Potential event queue overflow in USB stack. |
| F-901 |
Inference sync mode randomly freezes acquisition. |
| F-1010 |
Auto-exposure max gain limit is wrong. |
| F-904 |
InferenceNetworkName is not reset during factory reset. |
| F-897 |
GPIO line inference threshold is not saved to userset. |
| F-926 |
Replace inference bicubic scaling with bilinear scaling. |
| F-5953 |
ExposureEnd event does not work after debugging or terminating a host test application. |
| F-1075 |
Auto white balance only works in outdoor conditions. |
| F-1098 |
Mono pixel formats not working correctly. |
| F-949 |
Uploaded file size does not change if a smaller file is uploaded. |
| F-1051 |
USB transmission intermittently stops. |
| F-943 |
NetworkType selection does not get saved to userset. |
| F-988 |
CCM does not preserve the correct white point. |
| F-1093 |
Bayer pixel formats should be disabled when ISP is on. |
| F-1016 |
Bayer pixel formats are labelled incorrectly. |
| F-902 |
When an invalid network is uploaded InferenceEnable node should be unchecked and locked. |
| F-5610 |
Cannot stream images from two or more cameras using NI Max. |
| Issue |
Description |
| F-542 |
Rapidly starting/stopping acquisition while using U3V events may make camera not responsive. |
| F-587 |
U1 and U2 USB power states are advertised but do not work. |
| F-594 |
Doing a firmware update may not work on some USB2 interfaces. |
| F-601 |
USB device location node is incorrect. |
| F-604 |
The USB link will sometimes go down after acquisition/transmission is ended in continuous acquisition mode. The failure occurs only when an active USB IN transfer is aborted. |
| F-991 |
Spurious small voltage spikes can be observed on digital IO line 0 during state transitions. |
| F-1042 |
There is a small (less than 1%) chance that camera will not re-enumerate after DeviceReset command is issued. |
| F-6115 |
Uploading network twice causes inference not to run. |
| F-6324 |
Chance of device hang when cancelling image transfer when using USB2. |