FFY-U3-16S2 Release Notes

Product Information

Product: FFY-U3-16S2

Firmware Version: 2106.0.17.0

Bugs Fixed

Bug Description
F-380 Toggling FrameStart TriggerMode on/off while acquisition is active distorts the transmitted images.
F-949 FileSize node sometimes not updated to correct value if a file is overwritten.
F-1146 New exposure time setting takes an extra frame to take effect in trigger mode.
F-4583 Default trigger selector must be FrameStart.
F-4584 Serial number sometimes becomes '0' when USB interface is disconnected/reconnected.
F-5455 Multi-frame acquisition mode may not work correctly when exposure time is greater than sensor readout time.
F-5456 Maximum frame rate is slightly higher than what is allowed by IMX296 sensor data sheet.
F-5610 Acquisition won't start with NI Max software when two or more FFY cameras are connected.
F-5953 U3V events may stop working after acquisition is abnormally terminated.

Changes

Change Description
[1] FFY-U3-16S2C firmware update.
[2] FFY-U3-16S2M firmware update.

Known Issues

Issue Description
F-542 Rapidly starting/stopping acquisition while using U3V events may make camera not responsive.
F-587 U1 and U2 USB power states are advertised but do not work.
F-594 Doing a firmware update may not work on some USB2 interfaces.
F-601 USB device location node is incorrect.
F-604 The USB link will very rarely go down after acquisition/transmission is ended in continuous acquisition mode. The failure can only occur when an active USB IN transfer is aborted.
F-991 Spurious small voltage spikes can be observed on digital IO line 0 during state transitions.
F-1042 There is a small (less than 1%) chance that camera will not re-enumerate after DeviceReset command is issued.