You are here: Release Notes
FLIR

Firefly®

FFY-U3-16S2C-DL

 

FFY-U3-16S2C-DL Release Notes

Product Information

Product: FFY-U3-16S2C-DL

Firmware Version: 1905.0004.083.000

Bugs Fixed

Bug Description
NA

Changes

Change Description
[1] FFY-U3-16S2C-DL initial firmware release for manufacturing mass production.

Known Issues

Issue Description
F-542 Rapidly starting/stopping acquisition while using U3V events may make camera not responsive.
F-587 U1 and U2 USB power states are advertised but do not work.
F-594 Doing a firmware update may not work on some USB2 interfaces.
F-601 USB device location node is incorrect.
F-604 The USB link will sometimes go down after acquisition/transmission is ended in continuous acquisition mode. The failure occurs only when an active USB IN transfer is aborted.
F-991 Spurious small voltage spikes can be observed on digital IO line 0 during state transitions.
F-1042 There is a small (less than 1%) chance that camera will not re-enumerate after DeviceReset command is issued.

 

5/8/2020
© 2015-2020 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Firefly® FFY-U3-16S2C-DL
Camera Reference