Image Format Control

Region Of Interest

An image region of interest (ROI) lets you specify a portion of the image so that after each image is acquired only the pixel information from the specified portion is processed.

Use the following features to specify the location and size of the ROI. All values are in pixels.

OffsetX - Horizontal offset from the origin to the ROI.

Width - Width of the image provided by the device. This reflects the current ROI. The maximum value of this feature takes into account horizontal binning, decimation, or any other function changing the maximum horizontal dimensions of the image and is typically equal to WidthMax minus OffsetX.

OffsetY - Vertical offset from the origin to the ROI.

Height - Height of the image provided by the device. This reflects the current ROI. The maximum value of this feature takes into account vertical binning, decimation, or any other function changing the maximum vertical dimensions of the image and is typically equal to HeightMax minus OffsetY.

Binning

Binning refers to the act of combining the signal from groups of photo-sensitive cells into a larger logical pixel. This is achieved by adding (additive). Binning is implemented in analog by the sensor.

Note: Changes to binning features can only be made while the camera is not streaming.

Use the BinningSelector to choose the binning engine. This affects both horizontal and vertical binning. The choices are:

All - the total amount of binning. In this mode, the camera adjusts the sensor/ISP binning to achieve the best image quality with the fastest frame rate.

Sensor - the portion of binning implemented in analog by the sensor. Binning done by the sensor usually results in a higher frame rate. Unless otherwise specified, or unsupported, binning is done by the sensor by default.

ISP - the portion of binning implemented digitally by the ISP. Unless otherwise specified, binning is done by the ISP if sensor binning is is unsupported or compromises image quality.

Use BinningHorizontalMode and BinningVerticalMode to choose the algorithm to perform the combination. The choices are:

Additive - The response from the combined cells are added, resulting in increased sensitivity (a brighter image).

Average - The response from the combined cells are averaged, resulting in increased signal to noise ratio. Some sensors do not support average binning.

Use BinningHorizontal and BinningVertical to set the number of cells to combine. Binning values reduce the resolution of the image by a corresponding factor. A value of 1 indicates no binning. This must be set to 1 for decimation to be active.

ADC Bit Depth

All camera sensors incorporate an analog to digital converter (ADC) to digitize the images.

The camera's ADC is configured to a fixed bit output. This is not the same as pixel bit depth. If the pixel format selected has fewer bits per pixel than the ADC output, the least significant bits are dropped. If the pixel format selected has greater bits per pixel than the ADC output, the least significant bits are padded and can be discarded by the user. Image data is left-aligned across a 2-byte format.

For example, for a 12-bit output, the least significant 4 bits are padded in order to fill 2 bytes (0xFFF0).

A 10-bit conversion produces 1,024 possible values between 0 and 65,472.

A 12-bit conversion produces 4,096 possible values between 0 and 65,520.

A 14-bit conversion produces 16,384 possible values between 0 and 65,532.

Some image sensors support multiple ADC bit depths. (Not all ADC bit depths are supported on all cameras.) A higher ADC bit depth results in better image quality but slower maximum frame rate. Stop acquisition then use the ADC Bit Depth control to make a selection. Supported ADC bit depths are also listed in the camera's specification table.

Test Pattern

The camera is capable of outputting continuous static images for testing and development purposes.

Use the TestPatternGeneratorSelector feature to choose which test pattern to control.

Sensor produces a test pattern that varies based on the image sensor.

Set the TestPattern feature to Off to disable the selected test pattern generator.

When Sensor is selected, create a test pattern by setting the TestPattern feature to Sensor Test Pattern.

When Pipeline Start is selected, the test pattern can be defined by a user uploaded image by setting the TestPattern feature to Injected Image. The image uploaded by this test pattern needs to be the same bit depth as the sensor ADC Bit Depth in an unpacked format.

The Variable Frame Sequence option generates a sequence of frames containing varying test patterns. The sequence resets at the start of acquisition.

Most image processing features (such as Gamma, Balance Ratio, and others) are still available when the test pattern is on and can alter the test pattern image. Some features for controlling the sensor do not affect the test pattern image, such as Exposure Time, Gain, and analog Black Level. It is recommended to turn Exposure Auto and Gain Auto Off when using a test pattern, as those features do not function properly when the test pattern is on.

Note that the test pattern generators must be set to Off to get the actual image data from the sensor.

Pixel Format

Format of the pixel provided by the camera. Use PixelFormat feature to select from a list of supported formats. (Not all formats are supported on all cameras.) Once a format is selected, the following values are derived:

PixelSize provides the total size in bits of the image's pixel. Note: the pixel size is limited by the pixel format, not the sensor.

PixelDynamicRangeMin is the minimum value that can be returned during the digitization process. This corresponds to the darkest value of the camera. For color cameras, this returns the smallest value that each color component can take.

PixelDynamicRangeMax is the maximum value that can be returned during the digitization process. This corresponds to the brightest value of the camera. For color cameras, this returns the largest value that each color component can take.

Note: On the color sensor, non-bayer pixel formats are supported with ISP enabled; and bayer pixel formats are supported with Isp disabled.

Single Channel 8-bit and 16-bit Formats

8-bit Formats Mono8 8-bit monochrome packed format
16-bit Formats Mono16 16-bit monochrome packed format

Note: For Mono16 - when ISP is off, the lower n bits of each pixel contain actual image data (where n is the ADC bit depth). For example, on FFY the ADC bit depth is 10-bit so when selecting mono16 on the lower 10 bits contain the image data. This may result in a slightly darker image.

When ISP is on, the bits in each pixel always use the full range of the selecting output pixel format so when selecting mono16 all 16 bits potentially contain image data.

Reverse X

When Reverse X is enabled, it horizontally flips the image sent by the camera. The region of interest is applied after flipping.

For color cameras, the bayer pixel format may be changed after flipping. For example, BayerRG16 is changed to BayerGR16.

Reverse Y

When Reverse Y is enabled, it vertically flips the image sent by the camera. The region of interest is applied after flipping.

For color cameras, the bayer pixel format may be changed after flipping. For example, BayerRG16 is changed to BayerGB16.

Summary Table

Name Interface Access Visibility Description
Sensor Width IInteger RO Expert Effective width of the sensor in pixels.
Sensor Height IInteger RO Expert Effective height of the sensor in pixels.
Width Max IInteger Expert Maximum width of the image (in pixels). The dimension is calculated after horizontal binning. WidthMax does not take into account the current Region of interest (Width or OffsetX).
Height Max IInteger Expert Maximum height of the image (in pixels). This dimension is calculated after vertical binning. HeightMax does not take into account the current Region of interest (Height or OffsetY).
Width IInteger Beginner Width of the image provided by the device (in pixels).
Height IInteger Beginner Height of the image provided by the device (in pixels).
Offset X IInteger Beginner Horizontal offset from the origin to the ROI (in pixels).
Offset Y IInteger Beginner Vertical offset from the origin to the ROI (in pixels).
Pixel Format IEnumeration Beginner Format of the pixel provided by the camera.
Pixel Size IEnumeration RO Expert Total size in bits of a pixel of the image.
Pixel Color Filter IEnumeration RO Expert Type of color filter that is applied to the image. Only applies to Bayer pixel formats. All others have no color filter.
Pixel Dynamic Range Min IInteger RO Expert Minimum value that can be returned during the digitization process. This corresponds to the darkest value of the camera. For color cameras, this returns the smallest value that each color component can take.
Pixel Dynamic Range Max IInteger RO Expert Maximum value that can be returned during the digitization process. This corresponds to the brightest value of the camera. For color cameras, this returns the biggest value that each color component can take.
ISP Enable IBoolean RW Expert Controls whether the image processing core is used for optional pixel format mode (i.e. mono). Enabling ISP consumes more power but is required for auto algorithms (such as exposure and gain) to work. Pixel format bit depths that are greater than the sensor ADC bit depth utilize the full value range per pixel. When ISP is disabled, raw sensor data is LSB aligned in each pixel.
Isp Enable Lock State ICategory RO Expert Category for the Isp Enable Lock State features.
Binning Selector IEnumeration Beginner Selects which binning engine is controlled by the BinningHorizontal and BinningVertical features.
Binning Horizontal Mode [Binning Selector] IEnumeration Expert
Binning Vertical Mode [Binning Selector] IEnumeration Expert
Binning Horizontal [Binning Selector] IInteger Beginner Number of horizontal photo-sensitive cells to combine together. This reduces the horizontal resolution (width) of the image. A value of 1 indicates that no horizontal binning is performed by the camera. This value must be 1 for decimation to be active.
Binning Vertical [Binning Selector] IInteger Beginner Number of vertical photo-sensitive cells to combine together. This reduces the vertical resolution (height) of the image. A value of 1 indicates that no vertical binning is performed by the camera. This value must be 1 for decimation to be active.
Reverse X IBoolean RW Expert Horizontally flips the image sent by the device. The region of interest is applied after flipping. For color cameras the bayer pixel format is affected. For example, BayerRG16 changes to BayerGR16.
Reverse Y IBoolean RW Expert Vertically flips the image sent by the device. The region of interest is applied after flipping. For color cameras the bayer pixel format is affected. For example, BayerRG16 changes to BayerGB16.
Test Pattern Generator Selector IEnumeration Selects which test pattern generator is controlled by the TestPattern feature.
Test Pattern [Test Pattern Generator Selector] IEnumeration Selects the type of test pattern that is generated by the device as image source.
Injected Image Width IInteger Beginner Width of the injected image pattern.
Injected Image Height IInteger Beginner Height of the injected image pattern.
ADC Bit Depth IEnumeration Beginner Selects which ADC bit depth to use. A higher ADC bit depth results in better image quality but slower maximum frame rate.

Image Format Control Features


Sensor Width

Effective width of the sensor in pixels.

Property Value
Name SensorWidth
Interface IInteger
Access RO
Unit
Visibility Expert
Value 1456

Sensor Height

Effective height of the sensor in pixels.

Property Value
Name SensorHeight
Interface IInteger
Access RO
Unit
Visibility Expert
Value 1098

Width Max

Maximum width of the image (in pixels). The dimension is calculated after horizontal binning. WidthMax does not take into account the current Region of interest (Width or OffsetX).

Property Value
Name WidthMax
Interface IInteger
Access
Unit
Visibility Expert

Height Max

Maximum height of the image (in pixels). This dimension is calculated after vertical binning. HeightMax does not take into account the current Region of interest (Height or OffsetY).

Property Value
Name HeightMax
Interface IInteger
Access
Unit
Visibility Expert

Width

Width of the image provided by the device (in pixels).

Property Value
Name Width
Interface IInteger
Access
Unit
Visibility Beginner

Height

Height of the image provided by the device (in pixels).

Property Value
Name Height
Interface IInteger
Access
Unit
Visibility Beginner

Offset X

Horizontal offset from the origin to the ROI (in pixels).

Property Value
Name OffsetX
Interface IInteger
Access
Unit
Visibility Beginner

Offset Y

Vertical offset from the origin to the ROI (in pixels).

Property Value
Name OffsetY
Interface IInteger
Access
Unit
Visibility Beginner

Pixel Format

Format of the pixel provided by the camera.

Property Value
Name PixelFormat
Interface IEnumeration
Access
Visibility Beginner

Enumeration Values
Mono8
Mono16
BayerGR8
BayerRG8
BayerGB8
BayerBG8
BayerGR16
BayerRG16
BayerGB16
BayerBG16
BGR8

Pixel Size

Total size in bits of a pixel of the image.

Property Value
Name PixelSize
Interface IEnumeration
Access RO
Visibility Expert

Enumeration Values
Bpp8
Bpp16
Bpp24

Pixel Color Filter

Type of color filter that is applied to the image. Only applies to Bayer pixel formats. All others have no color filter.

Property Value
Name PixelColorFilter
Interface IEnumeration
Access RO
Visibility Expert

Enumeration Values
None

Pixel Dynamic Range Min

Minimum value that can be returned during the digitization process. This corresponds to the darkest value of the camera. For color cameras, this returns the smallest value that each color component can take.

Property Value
Name PixelDynamicRangeMin
Interface IInteger
Access RO
Unit
Visibility Expert
Value 0

Pixel Dynamic Range Max

Maximum value that can be returned during the digitization process. This corresponds to the brightest value of the camera. For color cameras, this returns the biggest value that each color component can take.

Property Value
Name PixelDynamicRangeMax
Interface IInteger
Access RO
Unit
Visibility Expert

ISP Enable

Controls whether the image processing core is used for optional pixel format mode (i.e. mono). Enabling ISP consumes more power but is required for auto algorithms (such as exposure and gain) to work. Pixel format bit depths that are greater than the sensor ADC bit depth utilize the full value range per pixel. When ISP is disabled, raw sensor data is LSB aligned in each pixel.

Property Value
Name IspEnable
Interface IBoolean
Access RW
Visibility Expert

Isp Enable Lock State

Category for the Isp Enable Lock State features.

Property Value
Name IspLockState
Interface ICategory
Access RO
Visibility Expert

Binning Selector

Selects which binning engine is controlled by the BinningHorizontal and BinningVertical features.

Property Value
Name BinningSelector
Interface IEnumeration
Access
Visibility Beginner

Enumeration Values
All
Sensor

Binning Horizontal Mode

Property Value
Name BinningHorizontalMode [Binning Selector]
Interface IEnumeration
Access
Visibility Expert

Enumeration Values
Sum
Average

Binning Vertical Mode

Property Value
Name BinningVerticalMode [Binning Selector]
Interface IEnumeration
Access
Visibility Expert

Enumeration Values
Sum
Average

Binning Horizontal

Number of horizontal photo-sensitive cells to combine together. This reduces the horizontal resolution (width) of the image. A value of 1 indicates that no horizontal binning is performed by the camera. This value must be 1 for decimation to be active.

Property Value
Name BinningHorizontal [Binning Selector]
Interface IInteger
Access
Unit
Visibility Beginner

Binning Vertical

Number of vertical photo-sensitive cells to combine together. This reduces the vertical resolution (height) of the image. A value of 1 indicates that no vertical binning is performed by the camera. This value must be 1 for decimation to be active.

Property Value
Name BinningVertical [Binning Selector]
Interface IInteger
Access
Unit
Visibility Beginner

Reverse X

Horizontally flips the image sent by the device. The region of interest is applied after flipping. For color cameras the bayer pixel format is affected. For example, BayerRG16 changes to BayerGR16.

Property Value
Name ReverseX
Interface IBoolean
Access RW
Visibility Expert

Reverse Y

Vertically flips the image sent by the device. The region of interest is applied after flipping. For color cameras the bayer pixel format is affected. For example, BayerRG16 changes to BayerGB16.

Property Value
Name ReverseY
Interface IBoolean
Access RW
Visibility Expert

Test Pattern Generator Selector

Selects which test pattern generator is controlled by the TestPattern feature.

Property Value
Name TestPatternGeneratorSelector
Interface IEnumeration
Access
Visibility

Enumeration Values
Sensor
PipelineStart

Test Pattern

Selects the type of test pattern that is generated by the device as image source.

Property Value
Name TestPattern [Test Pattern Generator Selector]
Interface IEnumeration
Access
Visibility

Enumeration Values
Off
SensorTestPattern

Injected Image Width

Width of the injected image pattern.

Property Value
Name InjectedWidth
Interface IInteger
Access
Unit
Visibility Beginner

Injected Image Height

Height of the injected image pattern.

Property Value
Name InjectedHeight
Interface IInteger
Access
Unit
Visibility Beginner

ADC Bit Depth

Selects which ADC bit depth to use. A higher ADC bit depth results in better image quality but slower maximum frame rate.

Property Value
Name AdcBitDepth
Interface IEnumeration
Access
Visibility Beginner

Enumeration Values
Bit10