You are here: Installation Guide > Physical Interface > Lens Mounting
FLIR

Firefly®

FFY-U3-16S2M-DL

 

Lens Mounting

Lenses are not included with individual cameras.

Related Knowledge Base Articles
Selecting a lens for your camera

Back Flange Distance

The Back Flange Distance (BFD) is offset due to the presence of both a 1 mm infrared cutoff (IRC) filter (color models only) and a 0.5 mm sensor package window. These two pieces of glass fit between the lens and the sensor image plane. The IRC filter is installed on color cameras. The sensor package window is installed by the sensor manufacturer. Both components cause refraction, which requires some offset in flange back distance to correct.

For more information about the IRC filter, see Infrared Cut-Off Filters.

 

5/8/2020
© 2015-2020 FLIR® Integrated Imaging Solutions Inc.
All rights reserved.
Legal
| Contact Support

Firefly® FFY-U3-16S2M-DL
Camera Reference