Transport Layer Control

The Transport Layer control provides the following information:

Payload Size - the number of bytes transferred for each image (including chunk data).

USB3 Vision Tab - Message Channel - Channel ID used for the Message Channel.

U3v Version Major/Minor - USB3 Vision standard version.

U3V Capabilities - what the camera supports (SIRM, EIRM and IIDC2).

Max Command Transfer Length - the maximum supported commands that can be sent to the camera.

Max Ack Transfer Length - the maximum supported ack that can be sent to the camera.

Number of Stream Channels - the number of stream channels the camera supports.

Current Speed - the speed of the camera's interface (Super Speed, High Speed).

Summary Table

Name Interface Access Visibility Description
Payload Size IInteger Expert Provides the number of bytes transferred for each image or chunk on the stream channel.
USB3 Vision ICategory RO Beginner Category that contains the features pertaining to the USB3 Vision transport layer of the device.

Transport Layer Control Features


Payload Size

Provides the number of bytes transferred for each image or chunk on the stream channel.

Property Value
Name PayloadSize
Interface IInteger
Access
Unit
Visibility Expert

USB3 Vision

Category that contains the features pertaining to the USB3 Vision transport layer of the device.

Property Value
Name USB3Vision
Interface ICategory
Access RO
Visibility Beginner