Event Control
Event Features
Events allow you to get notified when the camera has performed something you might find interesting. Events are similar to the asynchronous communication but the difference is the initiator is the device.
For more information, see Using the Event Control Feature.
Once an event is turned on, it has its own XML area where it outputs the event's ID, timestamp, and any applicable event data.
Use EventSelector to choose an event, then use EventNotification to set the event On or Off.
Standard events to choose:
Exposure End - Event is sent every image when exposure end occurs. Event data includes: the event ID, timestamp, and frame ID.
Serial Port Receive - Event is sent every time the serial port receives data. Event data includes: the event ID, timestamp, length, and overflow.
Error - Event is sent every time an error occurs internally in the device. Event data includes: the event ID, timestamp, frame ID, and error code.
In addition, some models support event generation on input I/O transitions:
Line X Rising Edge - Event sent when a rising edge is detected on input line X.
Line X Falling Edge - Event sent when a falling edge is detected on input line X.
The lines that can be used for these events are Line0, Line2, and Line3. Multiple I/O events can be enabled at a time.
Note: An adjustment to the Debouncer value may be needed if fast transitions result in multiple events being triggered.
In order to verify that events are working, there is a Test Event Generate command that can be executed to allow you to trigger the camera to send a test event out.
Event Test - Event you can trigger to verify events are working properly. This is always enabled. Event data includes: ID and timestamp.
Summary Table
| Name | Interface | Access | Visibility | Description |
|---|---|---|---|---|
| Event Selector | IEnumeration | RW | Expert | Selects which Event to enable or disable. |
| Event Notification [Event Selector] | IEnumeration | RW | Expert | Enables/Disables the selected event. |
| Event Exposure End Data | ICategory | RO | Expert | Category that contains all the data features related to the Exposure End Event. |
| Event Error Data | ICategory | RO | Expert | Category that contains all the data features related to the Error Event. |
| Event Serial Port Receive Data | ICategory | RO | Expert | Category that contains all the data features related to the Serial Port Receive Event. |
| Event Test Data | ICategory | RO | Expert | Category that contains all the data features related to the Test Event. |
| Line0 Rising Edge Data | ICategory | RO | Guru | Data of the Line0 rising edge event. |
| Line0 Falling Edge Data | ICategory | RO | Guru | Data of the Line0 falling edge event. |
| Line2 Rising Edge Data | ICategory | RO | Guru | Data of the Line2 rising edge event. |
| Line2 Falling Edge Data | ICategory | RO | Guru | Data of the Line2 falling edge event. |
| Line3 Rising Edge Data | ICategory | RO | Guru | Data of the Line3 rising edge event. |
| Line3 Falling Edge Data | ICategory | RO | Guru | Data of the Line3 falling edge event. |
Event Control Features
Event Selector
Selects which Event to enable or disable.
| Property | Value |
|---|---|
| Name | EventSelector |
| Interface | IEnumeration |
| Access | RW |
| Visibility | Expert |
| Enumeration Values |
|---|
| Error |
| ExposureEnd |
| SerialPortReceive |
| Line0RisingEdge |
| Line0FallingEdge |
| Line2RisingEdge |
| Line2FallingEdge |
| Line3RisingEdge |
| Line3FallingEdge |
Event Notification
Enables/Disables the selected event.
| Property | Value |
|---|---|
| Name | EventNotification [Event Selector] |
| Interface | IEnumeration |
| Access | RW |
| Visibility | Expert |
| Enumeration Values |
|---|
| On |
| Off |
Event Exposure End Data
Category that contains all the data features related to the Exposure End Event.
| Property | Value |
|---|---|
| Name | EventExposureEndData |
| Interface | ICategory |
| Access | RO |
| Visibility | Expert |
Event Error Data
Category that contains all the data features related to the Error Event.
| Property | Value |
|---|---|
| Name | EventErrorData |
| Interface | ICategory |
| Access | RO |
| Visibility | Expert |
Event Serial Port Receive Data
Category that contains all the data features related to the Serial Port Receive Event.
| Property | Value |
|---|---|
| Name | EventSerialPortReceiveData |
| Interface | ICategory |
| Access | RO |
| Visibility | Expert |
Event Test Data
Category that contains all the data features related to the Test Event.
| Property | Value |
|---|---|
| Name | EventTestData |
| Interface | ICategory |
| Access | RO |
| Visibility | Expert |
Line0 Rising Edge Data
Data of the Line0 rising edge event.
| Property | Value |
|---|---|
| Name | EventLine0RisingEdgeData |
| Interface | ICategory |
| Access | RO |
| Visibility | Guru |
Line0 Falling Edge Data
Data of the Line0 falling edge event.
| Property | Value |
|---|---|
| Name | EventLine0FallingEdgeData |
| Interface | ICategory |
| Access | RO |
| Visibility | Guru |
Line2 Rising Edge Data
Data of the Line2 rising edge event.
| Property | Value |
|---|---|
| Name | EventLine2RisingEdgeData |
| Interface | ICategory |
| Access | RO |
| Visibility | Guru |
Line2 Falling Edge Data
Data of the Line2 falling edge event.
| Property | Value |
|---|---|
| Name | EventLine2FallingEdgeData |
| Interface | ICategory |
| Access | RO |
| Visibility | Guru |
Line3 Rising Edge Data
Data of the Line3 rising edge event.
| Property | Value |
|---|---|
| Name | EventLine3RisingEdgeData |
| Interface | ICategory |
| Access | RO |
| Visibility | Guru |
Line3 Falling Edge Data
Data of the Line3 falling edge event.
| Property | Value |
|---|---|
| Name | EventLine3FallingEdgeData |
| Interface | ICategory |
| Access | RO |
| Visibility | Guru |