Configuring the Camera Driver

The driver is installed automatically by the Spinnaker SDK installer for Camera Evaluation or for Application Development if the Drivers checkbox is selected (default). A restart is required.

Note: For optimal driver performance, install Spinnaker version 4.0 or later.

Alternatively, you can manually install the driver. The driver files are located in:

C:\Program Files\Teledyne\GigE Vision Interface\x64

To manage and update drivers use the SpinView application:

  1. Start SpinView:
  2. Start MenuÒTeledyne Spinnaker SDKÒSpinView
  3. From the Devices list, select the camera and click the Switch Driver button.
  4. Select the driver from the drop-down list.
  5. Click Install Driver.