Configuring the Camera Driver

For the Oryx camera, ensure that PGRLWF driver version 2.7.3.92 or above is installed.

The PGRLWF driver should already be installed automatically using the Spinnaker SDK installer when the Camera Evaluation option is selected. Or in the case of Application Development option, the driver is installed if you select the GigE Driver checkbox.

Alternatively, you can manually install the driver. The PGRLWF files are located in:
C:\Program Files\FLIR Systems\Spinnaker\driver64

To verify your driver:

  1. Launch SpinView:
  2. Start-->All Programs-->Spinnaker SDK-->SpinView

  3. Select the camera.
  4. In the Feature tree search box, enter "driver". The Device Driver Version feature is highlighted.
  5. If you need to update the driver, right-click on the device and select Filter Driver Configuration.
  6. In the Filter Driver Configuration window, ensure the driver is installed and enabled. Click Refresh if making changes.
  7. Note: If the filter driver is not installed, a caution icon appears next to the device. Right-click on the device and select GigE Filter driver is not installed-->Install filter driver to resolve.