Mounting Your Oryx
Using the Case
The case is equipped with the following mounting holes:
- Four (4) M4.0 x 0.7 mounting holes on each side of the case
- One (1) 1/4-20 UNC mounting hole on the bottom of the case (standard and large case only)
Note: The 97-02800-00100 model is intended to be mounted to a fixed customer-designed bracket inside a camera array no more than 2 meters high. Using the model outside of this design is not recommended.
Using the ACC-01-0018 Mounting Bracket (small case only)
The tripod mounting bracket is equipped with four (4) M2 mounting holes.