Functions | |
class | DEPRECATED_CLASS ("AVIRecorder is deprecated, use SpinVideo instead.") SPINNAKER_API AVIRecorder |
Provides the functionality for the user to record images to an AVI file. More... | |
class Spinnaker::DEPRECATED_CLASS | ( | "AVIRecorder is | deprecated, |
use SpinVideo instead." | |||
) |
Provides the functionality for the user to record images to an AVI file.
NOTE: This class is deprecated and replaced by SpinVideo. Refer to SpinVideo.h instead.
Default constructor.
Default destructor.
Open an AVI file in preparation for writing Images to disk. The size of AVI files is limited to 2GB. The filenames are automatically generated using the filename specified.
pFileName | The filename of the AVI file. |
pOption | Options to apply to the AVI file. |
Open an MJPEG AVI file in preparation for writing Images to disk. The size of AVI files is limited to 2GB. The filenames are automatically generated using the filename specified.
pFileName | The filename of the AVI file. |
pOption | MJPEG options to apply to the AVI file. |
Open an H264 MP4 file in preparation for writing Images to disk. The size of MP4 files is limited to 2GB. The filenames are automatically generated using the filename specified.
pFileName | The filename of the MP4 file. |
pOption | H264 options to apply to the MP4 file. |
Append an image to the AVI/MP4 file.
pImage | The image to append. |
Close the AVI/MP4 file.
Set the maximum file size (in megabytes) of a AVI/MP4 file. A new AVI/MP4 file is created automatically when file size limit is reached. Setting a maximum size of 0 indicates no limit on file size.
size | The maximum AVI file size in MB. |
Contact Support | Spinnaker® SDK Programmer's Guide and API Reference | Tue Dec 19 2023 © FLIR Integrated Imaging Solutions Inc. All rights reserved. |