Mounting Your Blackfly S
Using the Case
The case is equipped with the following mounting holes:
- Two (2) M2 x 2 mm mounting holes on the top of the case
- Three (3) M3 x 2.5 mm mounting holes on the bottom of the case
- Four (4) M2 x 2 mm mounting holes on the bottom of the case that can be used to attach the camera directly to a custom mount or to the tripod mounting bracket
Using the Mounting Bracket
The tripod mounting bracket is equipped with four (4) M2 mounting holes.
Tripod Adapter Dimensions
Tripod Adapter Dimensional Diagram |
Tripod Adapter Dimensional Diagram |