Mounting Your Blackfly S
Using the Case
The case is equipped with the following mounting holes:
- Two (2) M2 x 2 mm mounting holes on the top of the case
- Three (3) M3 x 2.5 mm mounting holes on the bottom of the case
- Four (4) M2 x 2 mm mounting holes on the bottom of the case that can be used to attach the camera directly to a custom mount or to the tripod mounting bracket
Using the Mounting Bracket
The tripod mounting bracket is equipped with four (4) M2 mounting holes.
Tripod Adapter Dimensions
![]() |
![]() |
Tripod Adapter Dimensional Diagram |
Tripod Adapter Dimensional Diagram |